AXIS#.DISTO

Description

This timer starts when AXIS#.DIS is issued (regardless of the AXIS#.DIS origin). After this timeout elapses, the actual state of the drive is compared to the AXIS#.DISMODE setting. If the actual state does not match the AXIS#.DISMODE setting, a fault is reported and the hardware immediately executes the AXIS#.DISMODE setting (for instance, disable or activate dynamic brake). Setting AXIS#.DISTO to 0 will disable the timeout.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

0 to 120,000 ms

Default Value

1,000 ms

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.DISTO

5000h

09h

Unsigned32

-

-

Read/Write

No

AXIS2.DISTO

5100h

09h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.DISTO

5010

1392

Unsigned32

Read/Write

-

AXIS2.DISTO

70546

1139

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.DISTO

5010

Unsigned32

Read/Write

-